IRVINE, Calif. (April 25, 2019) - L-com, an Infinite Electronics brand and a preferred manufacturer of wired and wireless connectivity products, has expanded its line of outdoor industrial Ethernet cables to include additional sizes for use in industrial Ethernet, manufacturing, process industry, outdoor and direct burial applications.
These new extended size options are offered for several of L-com’s outdoor industrial Ethernet cable types, including Category 6a shielded, Category 6, Category 6 shielded, Category 5e and Category 5e shielded. They feature a polyethylene (PE) jacket that provides UV and moisture protection outdoors, with some also boasting a CMX UL burn rating. All series are available off the shelf in 1, 3, 5, 10, 15, 25, 50, 75, 100, 125, 150, 175, 200, 225 and 250 feet lengths. Custom lengths are available upon request.
“By offering extended off-the shelf sizes, in addition to custom lengths, all available with same-day shipping, we are able to provide our customers with more readily available, quality options to fulfill all of their outdoor industrial Ethernet cable needs,” said Dustin Guttadauro, Product Manager.
These outdoor-rated cables feature 23 AWG or 24 AWG solid conductors that are excellent for PoE and PoE+ applications. All families are designed to support Ethernet cable runs outside and are moisture and UV resistant. They are EIA568 color-coded for compatibility with standard installations. Operating temperatures range from -40°C to +75°C and depending on the cable type, some are suitable for direct burial. Shielded versions feature an overall foil shield to protect against EMI/RFI interference.
These outdoor industrial Ethernet cables are in-stock and available for immediate shipment.
For inquiries, L-com can be contacted at +1-978-682-6936
About L-com:
L-com, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. L-com is an Infinite Electronics brand.
About Infinite Electronics:
Infinite Electronics is a leading global supplier of electronic components serving the urgent needs of engineers through a family of highly recognized and trusted brands. Our portfolio brands are specialists within their respective product set, offering broad inventories of engineering-grade product, paired with expert technical support and same-day shipping. Over 100,000 customers across a diverse set of markets rely upon Infinite Electronics to stock and reliably ship urgently needed products every day.
For more information about this release, please contact:
Peter McNeil
L-com
17792 Fitch
Irvine, CA
978-682-6936