To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Expands Polycarbonate, NEMA-Rated Equipment Enclosure Line

Tuesday, February 22, 2022

L-com, an Infinite Electronics brand and a supplier of wired and wireless connectivity products, recently announced that it has expanded its line of polycarbonate NEMA-rated equipment enclosures, offering 46 new models.

L-com’s new polycarbonate NEMA enclosures are perfect for protecting equipment in both indoor and outdoor installations and can be used in wired and wireless networks. They are 12 inches by 10 inches by 6 inches and made of high-impact, UV-resistant polycarbonate material that is durable yet lightweight. They are well suited for hot or corrosive environments.

Options include gray and black colors, IP66 NEMA 4X and IP24 NEMA 3R ratings, nonpowered and powered models, and cooling and heating features. Some NEMA enclosures have clear lids to view the operational status of internal equipment. Additional features include a stainless-steel latch with padlock eye, fully gasketed lids and user-installed wall mounting brackets.

“The addition of these new polycarbonate enclosures further builds upon our extensive line of NEMA enclosure options, offering our customers rugged enclosure solutions to address every application. In addition to the many off-the-shelf enclosures we now offer, we are able to build custom enclosures to meet our customers’ specific project requirements," said William DiBella, Product Manager.

L-com stocks a wide range of polycarbonate NEMA enclosures to address a multitude of applications where protecting valuable equipment from theft, industrial environments and weather extremes is imperative. Off-the-shelf options include 120VAC and 240VAC power, heating, cooling, equipment mounting plates, DIN rail mounts and more.

L-com’s new 12x10x06-inch polycarbonate NEMA enclosures are in-stock and available for immediate shipment.

View L-com’s full range of polycarbonate enclosures or if you prefer a fiberglass enclosure, then check out our lineup of these weatherproof boxes as well.

About L-com:
L-com, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2015 certified and many of its products are UL® recognized. L-com is an Infinite Electronics brand.

About Infinite Electronics:
Based in Irvine, Calif., Infinite Electronics offers a broad range of components, assemblies and wired/wireless connectivity solutions serving the aerospace/defense, industrial, government, consumer electronics, instrumentation, medical and telecommunications markets. Infinite’s brands include Pasternack, Fairview Microwave, L-com, MilesTek, ShowMeCables, NavePoint, INC Installs, Integra Optics, PolyPhaser, Transtector, KP Performance Antennas, RadioWaves and Aiconics. Infinite Electronics serves a global engineering customer base with deep technical expertise and support, with one of the broadest inventories of products available for immediate shipment.

###

Press Contact:

Peter McNeil
L-com
17792 Fitch
Irvine, Calif. 92614
978-682-6936