NORTH ANDOVER, MA – 2/23/2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, has increased USB 2.0 type B connector options with two new styles of its very popular USB ECF coupler/cables. The new ECF504-xxBBS and ECF504-B-5M are similar to the existing ECF504-xxAAS and ECF504-5M products.
“We knew the type A USB versions were wildly popular,” said Steve Smith, Product Manager. “But until now we had no option with the type B USB jack in a flange-mount ECF option. Now we’re offering both as off-the-shelf products.”
The ECF504-xxBBS allows the user to panel-mount the female B connector on their product for easy accessibility and connect the male B connector end securely and easily inside their product. The ECF504-B-5M is used similarly but allows the user to cut the cable pigtail to the desired length and hard-wire or terminate with the connector of choice.
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, Inc, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized. https://www.L-com.com/