![]()
NORTH ANDOVER, MA - 11/13/14 - L-com Global Connectivity, a designer and manufacturer of wired and wireless connectivity products, announced today that they are now manufacturing
panel mount USB cables with ground wires. These USB 2.0 panel mount cables are perfect for use inside a box or enclosure.
By adding a ground wire, the user has the option to electrically ground the USB female connector to their panel or enclosure.
The molded panel mountable construction is rugged and robust; using 20 AWG power conductors and a 28 AWG twisted pair data conductors all under a double shield for maximum EMI resistance.
"We engineered these USB cables with ground wires to offer our customers adjustability and alternative design for their USB application," said Steve Smith, Product Manager. "These cables are a great fit in applications with limited space."
The new USB cables are available in lengths of 0.3, 0.5, 0.75, 1, 2, and 3 meters. The cable color is light gray and each assembly includes two 4-40 x 3/8" Phillips pan head mounting screws. The #6 spade lug easily attaches to a screw or similar hardware.
Common applications that use panel mountable USB cables include: PC Peripheral Interconnects, Test and Measurement, Data Acquisition, Portable Data Storage and
printer interface applications.
For more information about this release, please contact:
Lindsey Cook, Internet Marketing Specialist
978-682-6936 x1148, lcook@l-com.com
About L-com Global Connectivity
L-com Global Connectivity, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink®, L-com's other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions and Aiconics®, a leading manufacturer of electrical connector products. Trusted for over 30 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized For more information, please visit: https://www.L-com.com/
###