NORTH ANDOVER, MA – (May 24, 2011) – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, has expanded its line of USB 2.0 type B panel-mount assemblies with two new styles of coupler cables. They are the ECF504-xxBBS products (a female panel-mount connector to a male type B connector) and the ECF504-B-5M products (a female panel-mount coupler with 5-meter cable). “The type A USB versions were very popular with our customers, but until now we’ve had no cable assembly option with the type B USB jack in a flange-mount ECF option,” said Steve Smith, product manager. “Now we’re offering both as off-the-shelf products, which, combined with the flexibility, ease-of-use and reliable connections, should put these products in high demand.” The ECF504-xxBBS products feature a bulkhead Type B jack to a molded Type B plug attached via USB 2.0-compliant cable. These cables can be directly connected to a mating connector inside an enclosure. Screw mounting ensures secure installations and 30 micro inch gold-plated contacts provide reliable connections with repeated mating cycles. The assemblies are fully shielded and the ECF504-style housing can be used with virtually any panel thickness. The ECF504-xxBBS is available in lengths of 12, 24, 36, 72, and 120 inches, and custom lengths are available upon request with minimal quantity requirements. The ECF504-B-5M product is unique in that it allows users the flexibility to configure their own assemblies. The products feature a shielded bulkhead Type B jack with 5 meters of unterminated USB 2.0-compliant cable. The user can cut the cable to the desired length and hard wire or terminate it with their connector of choice. These also screw-mount for secure installations and have 30 microinch gold-plated contacts that ensure reliable connections with repeated mating cycles. This assembly is fully shielded and also usable in virtually any panel thickness. L-com can custom-terminate these cable ends with modest minimum requirements. For more information on this antenna, please call 1-800-341-5266. About L-com L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/. |