NORTH ANDOVER, MA, -- June 12, 2009 -- L-com, a global leader in the manufacture of wired and wireless connectivity solutions, has developed three new Category 5E high power, mid-span PoE injectors which provide data and power over a single Cat5 or Cat5E cable.
These new PoE injectors are 802.3af compliant and feature surge protection on all lines. In addition to the standard model, BT-CAT5E-P1-HP, L-com offers a 48 Watt power version , BT-CAT5E-P1-HP-4848, as well as a 70 Watt power version BT-CAT5E-P1-HP-4870.
“By combining surge protection on our PoE injectors we can offer our customers an extra level of protection in their investment over other competitors PoE injector products. Also we have addressed the need for higher power applications with the 4848 and 4870 kits which ship with the power supplies,” said Greg Pepin, Product Manager.
For more information about this release, please contact:
Greg Pepin, Product Manager
978-682-6936 x1186, gpepin@L-com.com
About L-com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.L-com.com