To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Global Connectivity Releases 802.3af Compliant NEMA Enclosures with Fans

Tuesday, June 16, 2009

NORTH ANDOVER, MA – June 17, 2009 – L-com, a global leader in the manufacture of wired and wireless connectivity solutions, today announced the addition of four new 802.3af compliant Power-over-Ethernet (PoE) NEMA rated weatherproof equipment enclosures.

The vented fiberglass enclosures feature thermostatically controlled cooling fans that can be powered by an PoE switch, midspan or injector.  The enclosures feature a aluminum mounting plate for user equipment. The plate features tapped holes for various popular network appliances. The 802.3af interface and thermostat used for fan control are mounted on the back of the plate. The base models feature a bi-metallic thermostat and two models feature a Solid State temperature controller for improved reliability and set-point accuracy. The majority of 802.3af compliant switches, midspans or injectors operating in Mode A or B can power the enclosures fans. This eliminates the need for a separate passive injector required by other L-com PoE NEMA enclosure models.  These rugged enclosures are perfect for both wired and wireless equipment installations in harsh, unforgiving environments both indoors and outdoors where dust or moisture is present. 

Two of the enclosures measure 14” X 12” X 7” and feature a single high CFM cooling fan. The other two enclosures in the series measure 18” X 16” X 8” and feature dual high CFM cooling fans. 

 

 

 

 

For more information about this release, please contact:
Karl Blomgren, Product Manager
561.995.2256 x7183, kblomgren@hyperlinktech.com

About L-com

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures.  L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.l-com.com