To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Global Connectivity Releases Right Angle USB Adapters to Address Tight Fit Applications

Wednesday, May 6, 2009

North Andover, MA – May 7, 2009 –  L-com, a global leader in the manufacture of wired and wireless connectivity products today announced that it now offers low profile right angle USB adapters to address tight fit applications. The UADAA90-1 and UADAA90-2 are constructed of durable molded PVC and are 100% shielded throughout to protect against data corrupting EMI/RFI.  

“These new right angle USB adapters are perfect for applications where cable assembly clearance is an issue. Also our new design is a lower cost solution to rotating USB adapters found on the market today,” said Steve Smith L-com’s USB Product Manager. 

Two exit options are available allowing cables to exit in opposite directions.

 

 

   

 

For more information about this release, please contact:
Steve Smith, Product Manager
978-682-6936 x1156, ssmith@L-com.com

About L-com

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures.  L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.l-com.com