L-com Introduces a 802.3af PoE Splitter/Tap with Adjustable DC Output NORTH ANDOVER, MA - 02/06/13 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has released a new Power-over-Ethernet (PoE) splitter/tap with a DC output that can be set to 5V, 7.5V, 9V, or 12V. The adjustable DC output allows these units to be used with a wide range of non-PoE devices such as wireless access points and IP cameras. The BT-CAT5-R0512 splitter/tap delivers both data and DC power to non-PoE equipped Ethernet devices using a single CAT5 cable. The unit supports both Fast and Gigabit Ethernet speeds. In addition, the BT-CAT5-R0512 is compliant with 802.3af PoE. The unit is unique in that it works with both 802.3af compliant network switches (PoE Mode A) and Midspan/Injectors (PoE Mode B). "Part of the convenience of PoE is the versatility to power remote electronics without needing to worry about the power availability at the location," said Patrick Pesa, Product Manager. "We just increased that versatility by allowing installers to choose the appropriate Voltage on a single PoE tap." Along with the units, L-com includes an 18-inch DC power cable along with 2.1mm and 2.5mm DC plugs in both straight and right angle configurations as part of a full kit. L-com provides free downloads of a datasheet, diagram 2D engineering drawing, and a 3D CAD model from its website. For a high-res version of the image suitable for print publication, follow this link, right click on the image, and select Save As: https://www.l-com.com/lcom_emails/2013/020613/BT_CAT5_R0512_2.jpg For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1169, dfallon@l-com.com L-com®, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the audio/video, OEM, military/aerospace, IT, and wireless RF industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the HyperLink® line of wireless antennas, amplifiers, filters/splitters, lightning protectors, weatherproof enclosures, and much more. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Massachusetts, USA, and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/ ### |