North Andover, MA -- April 23rd, 2008 -- L-com Inc. of North Andover, MA, has announced the availability of the new CSMNB, DB9 and DB25 black cable assemblies. Previously only available as custom cable assemblies, these robust yet economical cables are now available off the shelf and ready to ship the same day!
These assemblies are fully shielded throughout the entire cable to prevent against data corrupting EMI/RFI. Molded backshells provide superior strain relief while 26 AWG conductors are wired straight through for ease of compatibility. Metal thumbscrews insure fast and easy connections. Standard lengths range from 2.5 ft to 50 ft and both male to male and male to female versions are offered.
For more information about this release, please contact:
Steve Smith
Product Manager
Direct Line: 1-978-682-6936 x156
Email Address: ssmith@l-com.com
About L-com
Founded in 1982, L-com is dedicated to the design and production of a wide range of interconnect products for the electronics and data communications industries. Its primary products include cables and accessories for IEEE488 systems, modular and coaxial, and computer networking. The company markets directly, and succeeds by providing a wide breadth of in-stock, difficult-to-find products and serving a broad customer base. The company leverages its design capabilities by offering customized solutions, which have led to the development of many new products, many of which are proprietary.