North Andover, MA – May 21st, 2008 – L-com announced today that it will carry its own line of latching and non-latching Category 6 rated A/B switch boxes. These robust switch boxes feature a unique relay technology that supports the switching mechanism. The non-latching units provide automatic fail-over to the default Port A to C connection state when power fails or is removed. Latching relays provide the benefit of maintaining the flow of data between the connected devices even when power is removed. Additionally, all units incorporate a proprietary physical interface that enables these switch boxes to meet or exceed the stringent requirements of the Category 6 specification allowing support of 10/100/1000Mbps Ethernet data rates.
For more information about this release, please contact:
Greg Pepin, Product Manager
978-682-6936 x186, gpepin@L-com.com
![]()
![]()
About L-com
Founded in 1982, L-com is dedicated to the design and production of a wide range of interconnect products for the electronics and data communications industries. Its primary products include cables and accessories for IEEE488 systems, modular and coaxial, and computer networking. The company markets directly, and succeeds by providing a wide breadth of in-stock, difficult-to-find products and serving a broad customer base. The company leverages its design capabilities by offering customized solutions, which have led to the development of many new products, many of which are proprietary.