L-com Introduces Complete Line of DIN 3 Rail Mountable Lightning Protectors NORTH ANDOVER, MA – November 10, 2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, now carries a line of DIN rail mountable lightning and surge protectors. The new products come in models that protect Cat5, Cat5e and Cat6 lines; RS-422 and RS-485 lines; telephone/DSL/T1 lines; and 4-20 mA current loop lines. The new lightning protectors are designed to mount onto DIN 3 rail systems, such as those used in L-com’s NEMA rated DIN rail waterproof enclosures. L-com’s DIN mounted protectors are easily integrated in DIN rail systems without the need of drilling holes into the racks and cabinets, saving much time and effort. “DIN mountable equipment can be quickly and easily installed and configured,” said Patrick Pesa, Director of Product Development. “Our lightning protectors are already among the highest quality available; now they are highly convenient, too.” L-com will manufacture these new lightning protectors in the USA. Prices for most models will start under $50. For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1450, newsletters@L-com.com L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/ |