NORTH ANDOVER, Mass. (September 17, 2015) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, has introduced a series of antennas that have been specifically designed for Distributed Antenna System (DAS) applications.
L-com’s HyperLink brand HG727 series antennas can provide coverage from 700 MHz to 2700 MHz in a single antenna package, which enables them to support networks that include cellular 4G/LTE, personal communication services (PCS) and 802.11 Wi-Fi connectivity. Combining all of these frequencies into a single antenna eliminates the need to purchase separate antennas to cover different wireless frequencies. Using DAS antennas simplifies installation and reduces deployment costs.
L-com’s DAS antenna offering includes ceiling mount, Omni-directional, sector and mobile mount style antennas to address a variety of fixed and mobile DAS applications.
"Our goal is to offer a comprehensive selection of antennas to support DAS installations," said Patrick Pesa, Director of Product Development. "These versatile antennas were designed to address both indoor and outdoor DAS applications that require wide frequency support along with strong signal coverage."
L-com’s DAS antennas are in stock and ready to ship. Detailed datasheets, diagrams, 2D engineering drawings and CAD models are available for download from L-com's website.
For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, mailto:pmcneil@l-com.com
About L-com Global Connectivity
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions and Aiconics®, a leading manufacturer of electrical connector products. Trusted for over 30 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit: https://www.L-com.com/