NORTH ANDOVER, Mass. (November 5, 2015) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has launched a dual-band 4x4 multiple-input multiple-output (MIMO) outdoor Omni-directional antenna.
L-com’s HyperLink® brand HG245806U-4-series antennas were developed to work seamlessly with popular new dual-band MIMO access points.
Unlike typical pole-style Omni-directional antennas, the HG245806U-4-series antenna features a compact and unobtrusive UV-resistant radome, making it durable and rugged. Designed specifically for MIMO applications, the HG245806U-4-series operates on both 2.4 GHz and 5.8 GHz frequencies, allowing the radio to select the optimal frequency for obtaining the highest data rates.
“The HG245806U-4-series is a new type of antenna that is able to support the new IEEE 802.11ac standard as well as the existing 802.11a, 802.11b, 802.11g, and 802.11n standards. It is ideal for use with 4x4 MIMO radios because it features four separate 3-foot antennas leads. Each lead is dual-band and supports both 2.4 GHz and 5.8 GHz bandwidths,” said Ken Burgner, Product Manager.
This antenna features a modern design to help it blend into most environments and structures, and is available with either RP-TNC plug connectors or RP-SMA plug connectors.
For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, mailto:pmcneil@l-com.com
About L-com Global Connectivity
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions and Aiconics®, a leading manufacturer of electrical connector products. Trusted for over 30 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit: https://www.L-com.com/