To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com introduces eight new HyperLink brand “OEM” 2.4 GHz Wi-Fi Amplifier models

Monday, June 23, 2008

North Andover, MA – June 24, 2008 – L-com Global Connectivity is pleased to announce twelve new “OEM” Wi-Fi amplifiers to its current RF amplifier line. These new models are ideal for OEM type applications.

802.11b/g and 802.11b/g Wi-Fi OEM Amplifiers with Low Profile SMA Connectors

L-com's HA2401SFGI series amplifiers feature low profile SMA-Female connectors. This helps reduce the overall height of the amplifier, making it ideal for installations with limited space. These amplifiers feature cast aluminum construction and are available in 100 mW, 250 mW, 500 mW and 1 Watt models.

For Power-Over-Ethernet (PoE) applications, there are the HA2401SFGE series amplifiers. Like the HA2401SFGI amplifiers, this series also feature the low profile SMA-Female connectors. In addition, the HA2401SFGE series amplifiers feature an integral PoE interface. This allows the amplifier to receive its power by the same CAT5 cable used to pass Data and Power to products such as Access Points with PoE capability.

For more information about this release, please contact:
Ken Burgner, Product Manager
561-995-2256 x7140, kburgner@hyperlinktech.com

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures.  L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.l-com.com