NORTH ANDOVER, MA – 1/12/2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, has released new 20AWG (American Wire Gauge) D-Subminiature cables, designed for ultra-durability due to the heavier wire. 20AWG conductors will also allow for maximum current to pass through the cable. "After receiving many requests for D-Sub cables with larger AWG conductors, we now have them available off-the-shelf for same-day shipping," said Steve Smith, Product Manager. The cables are available in male-to-male and male-to-female versions, with DB9-, DB15-, and DB25-style molded connectors on the ends. In addition to the thicker conductors, the connectors will also be double-shielded to help reduce electromagnetic interference (EMI). For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1450, newsletters@L-com.com To see all of our press releases, click here. L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, Inc, which is headquartered in North Andover, MA, is ISO 9001:2008 certified and many of its products are UL® recognized. https://www.L-com.com/ | |