L-com Introduces HyperLink® Spatial Diversity/Cross Polarized Sectorial Panel Antennas ![]()
NORTH ANDOVER, MA – 11/07/13 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, announced today that it has introduced two new
HyperLink® brand 2.4 GHz Spatial Diversity/Cross Polarized Sectorial Panel Antennas. These outdoor all weather antennas are designed with two identical and independent internal cross polarized antennas fed via four connectors.
The spatial diversity feature of these antennas is useful for operating in areas susceptible to the effects of multi-path interference. By providing spatial diversity, the radio's internal circuitry can select between the two receive antennas for better wireless reception. In the case of 802.11n or MIMO, two or more spatially or polarization diverse antennas are required for the radio to operate at its highest data rate.
Additionally, inside each sector antenna enclosure are two independent cross polarized antennas. These cross polarized antennas double the wireless capacity over the same channels. Each of the two internal cross polarized antennas are fed via two N-Female ports, one for +45° polarized and one for -45° polarized signals. This feature makes this antenna ideal for polarization diversity systems.
“Our new Spatial Diversity, Cross Polarized antennas are perfect for use in areas plagued with multi-path interference. Their unique design makes them ideal for service providers operating in the 2.4 GHz ISM band,” said Ken Burgner, Wireless Product Manager.
The two new antennas are listed below and can be ordered directly from the L-com.com web site or by calling L-com sales at 1-800-341-5266.
HG2412SXP-120 - 2.4 GHz, 12 dBi, 120 Degree Beam Width Spatial Diversity/Cross Polarized Sectorial Panel Antenna
HG2416SXP-090 - 2.4 GHz, 16 dBi, 90 Degree Beam Width Spatial Diversity/Cross Polarized Sectorial Panel Antenna
For a high-res version of these images suitable for print publication, follow this link, right click on the links and select Save As:
https://www.l-com.com/lcom_emails/2013/110713/HG2412SXP-120.jpg https://www.l-com.com/lcom_emails/2013/110713/HG2416SXP-090.jpg
For more information about this release, please contact:
Peter McNeil, Product Marketing Manager
978-682-6936 x1450, pmcneil@l-com.com
L-com®, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the audio/video, OEM, military/aerospace, IT, and wireless RF industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the HyperLink® line of wireless antennas, amplifiers, filters/splitters, lightning protectors, weatherproof enclosures, and much more. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Massachusetts, USA, and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/
###