L-com Introduces LSZH SATA Cables with Latching Connectors NORTH ANDOVER, MA - 07/15/13 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, now offers a version of serial ATA (SATA) cable assembly with a low-smoke, zero halogen (LSZH) jacket and latching 7-position connectors that resist vibration. The new cable assemblies are made for a variety of applications, especially military/aerospace, where vibration is common and ventilation is poor. LSZH cable jackets are commonly required in certain applications where, in the event of a fire, occupants may not be able to evacuate quickly. Common PVC jackets will burn readily and release toxic gas, sometimes overwhelming anyone nearby. LSZH material produces very little smoke and no toxic gases. Most SATA connectors are also designed for a "friction fit," meaning they mate by pushing the connector into the jack and can be unplugged simply by pulling. In high vibration applications, this can lead to the connector popping out of its jack unexpectedly. L-com's latching connectors will remain connected until the latch is depressed. "We already have one of the best selections of LSZH USB, audio/video, D-Subminiature, fiber optic and Ethernet cable assemblies in the industry," said Steve Smith, Product Manager. "Today, I'm happy to add these hard-to-find products that may be used in applications where PVC jackets and friction fit connectors must be avoided." L-com's new LSZH SATA cables are expected to start shipping by the end of July from L-com's North Andover, MA, fulfillment center. Detailed engineering drawings and 3D CAD models are available from L-com's website. For a high res version of this image, please follow this link, right click on the image and select Save As: https://www.l-com.com/lcom_emails/2013/071513/casatazl_.jpg For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1169, dfallon@l-com.com L-com®, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the audio/video, OEM, military/aerospace, IT, and wireless RF industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the HyperLink® line of wireless antennas, amplifiers, filters/splitters, lightning protectors, weatherproof enclosures, and much more. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Massachusetts, USA, and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/ ### |