NORTH ANDOVER, MA - 07/10/14 - L-com Global Connectivity, a designer and manufacturer of wired and wireless connectivity products, announced today that they are now offering three new HyperLink Cross Polarized Flat Panel Antennas in addition to their current product line. Inside each model are two independent antennas that are cross polarized, which doubles wireless capacity over the same channels.
"These new products offer amazing wireless capacity for a low price," said Kenneth Burgner, Product Manager, "Thanks to the quality of the HyperLink brand, we've continued to be the go-to supplier for these kinds of antennas."
Each antenna within the cross polarized flat panel is fed via two N-Female ports, one for +45° polarized and one for -45° polarized signals. This feature makes these antennas ideal for polarization diversity systems. Designed primarily for MIMO point-to-multipoint and point-to-point applications, these antennas can be used with access points and routers with one or two antenna ports.
These indoor/outdoor all-weather antennas are also lightweight and feature a durable aesthetic UV-stable, UL flame-rated white plastic radome, which can also be painted to match the room or building structure. Installation is made easy with integral mounting flanges.
The three new models that are available are as follows:
HG2409XP - 2.4 GHz 9 dBi Flat Panel Antenna
HG2458-11XP - 2.4/4.9-5.8 GHz 9/11 dBi Flat Panel Antenna
HG2458-15XP - 2.4/4.9-5.8 GHz 13/15 dBi Flat Panel Antenna
For more information about this release, please contact:
Lindsey Cook, Internet Marketing Specialist
978-682-6936 x1148, lcook@l-com.com
About L-com Global Connectivity
L-com Global Connectivity, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink®, L-com's other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions and Aiconics®, a leading manufacturer of electrical connector products. Trusted for over 30 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized For more information, please visit: https://www.L-com.com/
###