To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Introduces New Erbium-Doped Amplifiers and Transmitters for Long Haul Fiber Applications

Tuesday, September 14, 2021

L-com, an Infinite Electronics brand and a preferred manufacturer of wired and wireless connectivity products, announced today that it has launched a new series of Erbium-Doped Fiber Amplifiers (EDFA) and directly modulated fiber transmitters, providing a cost-effective solution for easy conversion and amplification of high-quality voice, video and data signals.

Typically used in applications that require long-distance optical fiber transmission of TV image signals, digital television signals, telephone voice signals and data (or compressed data) signals, these fiber amplifiers utilize erbium-doped fiber which offers high gain, wide bandwidth, high output power, high pumping efficiency, and low insertion loss. 

The new EDFA fiber amplifiers feature high-performance erbium-doped fiber with a low noise pump laser, embedded automatic monitoring system, AC power, 78 channels and an FC port. They operate on the 1550nm wavelength.

L-com’s new directly modulated fiber transmitters are available in both 1310nm and 1550nm wavelength versions and feature AC Power, one SC/APC connector and a wide automatic gain control (AGC) range in the 1.2 GHz band.

“Our new EDFA amplifiers and fiber transmitters are critical components for distributing and extending optical signals in CATV network applications. By using an erbium-doped design, these new products offer the highest levels of output power, gain and very low insertion loss, resulting in the highest quality output signals,” said Paul Hospodar, Product Line Manager.

L-com’s new EDFA fiber amplifiers and direct modulated fiber transmitters are in-stock and available for immediate shipment.

About L-com:

L-com, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2015 certified and many of its products are UL® recognized. L-com is an Infinite Electronics brand.

About Infinite Electronics:

Based in Irvine, Calif., Infinite Electronics offers a broad range of components, assemblies and wired/wireless connectivity solutions, serving the aerospace/defense, industrial, government, consumer electronics, instrumentation, medical and telecommunications markets. Infinite’s brands include Pasternack, Fairview Microwave, L-com, MilesTek, ShowMeCables, NavePoint, INC Installs, Integra Optics, PolyPhaser, Transtector, KP Performance Antennas, RadioWaves and Aiconics. Infinite Electronics serves a global engineering customer base with deep technical expertise and support, with one of the broadest inventories of products available for immediate shipment.

###

 

Press Contact:

Peter McNeil
L-com
17792 Fitch
Irvine, Calif. 92614
978-682-6936