To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Introduces New Flat HDMI Cables for Tight Space A/V Applications

Monday, July 16, 2018

NORTH ANDOVER, Mass. (July 17, 2018) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has introduced a new series of flat HDMI cables for use in Diagnostic equipment, gaming, professional A/V, medical and digital signage applications.

L-com's new flat HDMI cables offer a cost effective way to support HDMI applications in confined areas. The unique flat cable design allows users to easily route the cables around corners or in between tight spaces. 

Additional features include rugged over-mold connectors, PVC jacketing, gold plated contacts and double shielding which protects A/V signals from EMI/RFI. Furthermore, these flat high speed HDMI cables support 4K, 1080p resolution and are available off the shelf in six lengths ranging from .5 meters to five meters.

“L-com’s flat HDMI cables provide our customers with an option from standard round cables and can be pressed flat in tight areas providing valuable space within a device or installation area as well as enhance air flow.  These cables meet the HDMI industry performance specification and provide a flexible and streamlined connectivity solution,” said Brian Gates, Product Manager.

L-com’s new flat HDMI cables are in stock and available for immediate shipment.
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
L-com Global Connectivity, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. L-com is an Infinite Electronics company.

Search Entries: