To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Introduces New IP67 Category5e/6 Dual Use Waterproof Ethernet Cables

Sunday, April 8, 2018

NORTH ANDOVER, Mass. (April 9, 2018) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has launched a new series of IP67 rated waterproof Ethernet cables designed to address harsh environment networking applications.

The innovative design of L-com’s new IP67 waterproof cables allows them to be used with IP rated receptacles for a watertight seal or they can be used with standard RJ45 jacks. This eliminates the need to find specialized cables that are IP rated on one end and have a standard RJ45 on the other end. This dual functionality is accomplished by a waterproof shroud that can be pulled back to mate with standard RJ45 jacks.

Additional features include a foil shield to protect against EMI/RFI interference, a tethered dustproof shroud cap and a CMX outdoor burn rating. These versatile cables are available in both Category 5e and Category 6 versions and are compatible with L-com's WPBH series of RJ45 jacks for an IP67 rated seal.

“These new IP67 Ethernet cables provide the flexibility of being able to mate to standard or IP rated jacks meaning our customers can save time and money by purchasing just one assembly to address multiple application. The innovative design of these cables is sure to appeal to our industrial, military and transportation customers,” said Dustin Guttadauro, Product Manager.

L-com’s new IP67 waterproof Ethernet cable assemblies are in stock and available for immediate shipment.

For more information about this release, please contact:

Peter McNeil
L-com Global Connectivity
17792 Fitch
Irvine, CA
978-682-6936 x1174

About L-com Global Connectivity:

L-com Global Connectivity, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. L-com is an Infinite Electronics company.

Search Entries: