NORTH ANDOVER, Mass. (July 12, 2018) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has introduced a new line of waterproof HDMI cable assemblies for use in industrial computing, digital signage, factory automation, medical and harsh environment A/V applications.
These unique IP67 rated HDMI cables feature a waterproof coupling that allows the HDMI connectors to survive harsh environments by preventing the ingress of water and fine particulates such as dust that would typically debilitate standard HDMI connectors.
These unique cables feature support for 4K and 1080p resolutions, rugged molded backshells and gold plated contacts that stand up to repeated mating cycles.
In addition to the new waterproof HDMI cables, L-com has also released a new IP67-rated HDMI panel-mount coupler that can be used with the cable assemblies. The VHC00023 features a standard female HDMI Type-A connector on one side and PC tails on other side for termination to wire or a PC board.
“Our waterproof HDMI cables and coupler offer a perfect solution for our customers who require HDMI connectivity in harsh environments often found in industrial computing and display applications. These unique IP67 rated interconnects are available off-the-shelf with no minimum order quantities,” said Brian Gates, Product Manager.
L-com’s waterproof HDMI cables and panel-mount coupler are in stock and available for immediate shipment.
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
L-com Global Connectivity, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. L-com is an Infinite Electronics company.