To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Introduces New Line of 18 GHz, LL142 & LL335i Rugged Low-Loss Cables

Monday, March 2, 2020

L-com, an Infinite Electronics brand and a preferred manufacturer of wired and wireless connectivity products, announced today that it has launched a new series of flexible 18 GHz LL142 and LL335i low-loss cables. These new cable assemblies are terminated with durable stainless steel connectors and are well suited for test environments where a rugged, phase stable cable assembly is required.


L-com’s new low-loss cables utilize a 0.195 & 0.300 inch diameter coax with an expanded dielectric which results in 80% and 83% Velocity of Propagation (VoP) performance up to 18 GHz. These coaxial cable assemblies feature LL142 and LL335i coax cable, which operates at higher power with improved phase stability. The triple shielded flexible coax provides excellent shielding effectiveness greater than 95 dB and VSWR of less than 1.35:1. A heavy duty boot and FEP jacket improve strain relief and allow for a minimum bend radius of .945 and 1.5 inches which adds to the durability of these cable assemblies.

L-com’s new line of LL142 and LL335i test cables are offered with male-straight and right-angle versions of Type-N, SMA, and TNC connectors as well as female bulkhead versions for each connector series. These new cables can be ordered in custom lengths and are also available in standard lengths from 1 Ft to 10 Ft. Each assembly is 100% continuity, Hi-Pot and RF tested prior to shipment. Our coax tools are useful with the LL142 and LL335i test cables as well.

“These new cables offer our customers a high performance solution when requiring a low-loss cable assembly. The smaller diameter of these new 18 GHz coax cables provides a tighter bend radius while offering low loss and higher power when compared to solid dielectric cables,” said Steve Ellis, Product Line Manager.


L-com’s new 18 GHz,
LL142 and LL335i coaxial cables are all in-stock and available for immediate shipment.

About L-com:

L-com, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2015 certified and many of its products are UL® recognized. L-com is an Infinite Electronics brand.

About Infinite Electronics:

Based in Irvine, Calif., Infinite Electronics offers a broad range of components, assemblies and wired/wireless connectivity solutions, serving the aerospace/defense, industrial, government, consumer electronics, instrumentation, medical and telecommunications markets. Infinite’s brands include Pasternack, Fairview Microwave, L-com, MilesTek, Aiconics, KP Performance Antennas, PolyPhaser, Transtector, RadioWaves, ShowMe Cables, INC-Installs and Integra Optics. Infinite Electronics serves a global engineering customer base with deep technical expertise and support, with one of the broadest inventories of products available for immediate shipment.

###

Press Contact:

Peter McNeil
L-com
17792 Fitch
Irvine, CA
978-682-6936