NORTH ANDOVER, Mass. (April 14, 2016) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has launched two series of plenum-rated, low-PIM coaxial cable assemblies.
L-com’s RG401 and RG402 plenum-rated, low-PIM cable assemblies are constructed using jacketed, high-performance, formable RG401 or RG402 coaxial cable. These plenum-rated cable assemblies feature passive intermodulation (PIM) specifications as low as -150dBc and are ideal for applications that incorporate Distributed Antenna Systems (DAS). These cable assemblies are available with either 7/16 DIN Male or Type N-Male connectors.
“High levels of PIM in the transmission path directly result in poor performance of a DAS network. Our plenum-rated, low-PIM coaxial cable assemblies ensure strong signal and more bandwidth by limiting PIM in the connection between wireless components,” said Ken Burgner, Product Manager.
L-com’s RG401 and RG402 plenum-rated, low-PIM cable assemblies are built to order using an online cable configurator. The configurator allows customers to price and purchase cables that are designed to their specifications through L-com’s website. Customers can select the cable type, connectors, and length in inches, feet or meters. The configurator generates pricing for the custom cable, which can then be added to the online cart, allowing customers to order specifically what they need.
Low-PIM RG401 and RG402 bulk cable is also available by the foot for those who want to build their own cable assemblies. In addition to low-PIM cable and cable assemblies, L-com also offers low-PIM coax connectors, coax adapters, coax lightning protectors, and antennas.
For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, mailto:pmcneil@l-com.com
About L-com Global Connectivity
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit: https://www.L-com.com/