North Andover, MA – July 21, 2009 – L-com, a global leader in the manufacture of wired and wireless connectivity products announced today the release of a new 90 degree Cat 5E coupler. An exclusive product design from L-com, the new TDG1026KC-R5E right angle Category 5E coupler offers true 90° connectivity.
This unique keystone coupler was designed to address tight fit applications commonly seen with wall plates and some panel designs. The TDG1026KC-R5E Cat 5E coupler fits standard .765" X .585" keystone openings and can be used for myriad voice, video and data applications and meets Category 5E standards.
Additionally, L-com now offers a fully shielded version of this right angle RJ45 coupler.
For more information about this release, please contact:
Greg Pepin, Product Manager 978-682-6936 x1186, gpepin@L-com.com
About L-com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.l-com.com