![]()
NORTH ANDOVER, MA - 04/03/14 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, announced today that they have added one foot cable length options to their CHD Deluxe High Density D-Sub cables and CRMN Deluxe Panel Mount D-Sub cable lines. This will give customers the option of a more streamlined fit to achieve D-Sub connections in tight or confined space applications, at a reduced cost.
L-com's CHD family of hard-to-find high-density (HD) D-Sub cable assemblies offers solid performance at economical prices. These HD cable assemblies are fully shielded throughout the entire cable to prevent data corrupting EMI/RFI. Metal thumbscrews ensure fast and easy connections and custom lengths and pinouts are available with modest minimum requirements. One foot options have been added to the following product families: CHD15MF, CHD15MM, CHD26MF, CHD26MM, CHD44MF, CHD44MM, CHD62MF, CHD62MM, CHD78MF and CHD78MM.
L-com's CRMN D-Sub cable assemblies were the industry's first to feature connectors with threaded inserts. These allow either metal thumbscrews or female hex standoffs to be threaded securely to each connector. They are also fully shielded with molded backshells and 26 AWG conductors. One foot cable lengths have been added to the DB9, DB15, DB25, and DB37 sizes in male to male, male to female and female to female configurations.
"Adding shorter options has proven to be successful with our standard D-Sub cables as well as with other interfaces, so we wanted to make them available to those customers who require the CHD and CRMN products as well," said Steve Smith, Product Manager.
For more information about this release, please contact:
Peter McNeil, Product Marketing Manager
978-682-6936 x1450, pmcneil@l-com.com
L-com Global Connectivity, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink®, L-com's other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions and Aiconics®, a leading manufacturer of electrical connector products. Trusted for over 30 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit: https://www.L-com.com/
###