NORTH ANDOVER, Mass. (February 18, 2016) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has launched two new series of slim-line 28 AWG Ethernet patch cables.
L-com’s new slim-line 28 AWG Ethernet patch cables are engineered for high-density patching applications. The patent pending spline-free design offers a reduced diameter profile, ideal for applications that require a smaller, more flexible cable. The low-profile short boot design saves additional space on the patch panel, giving a clean, organized look to patch bays.
“L-com’s slim-line high-performance cable assemblies offer a 38% smaller cross-sectional area and a tighter bend radius than standard patch cables. This improves airflow in high-density patching applications and saves space in confined areas,” said Dave Gallagher, Product Manager.
These cables are available in performance ratings of Category 6 (TRD628BL-series) and Category 6A (TRD628ABL- series) and support data rates up to 10Gbps for high-speed voice, video, and data applications. They feature high-performance RJ45 plugs with molded boots and 50u gold plated contacts. The slim-line 28 AWG Ethernet patch cables are available off-the-shelf in lengths of 1 ft, 3 ft, 5 ft, 7 ft, 10 ft and 14 ft, and are also available in custom length and color variations.
For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, mailto:pmcneil@l-com.com
About L-com Global Connectivity:
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit: https://www.L-com.com/