NORTH ANDOVER, Mass. (August 18, 2016) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has released a ceiling-mount public safety DAS antenna.
L-com’s HyperLink brand HG35805CUPR-NF is an IP67-rated, multi-band, low-PIM, Omni-directional, ceiling-mount antenna specifically designed for in-building wireless networks. With coverage from 380 MHz to 6000 MHz, this antenna is ideal for standard and public safety Distributed Antenna Systems (DAS) used to disseminate Cellular/LTE and Wi-Fi signals throughout an area or building.
“The HG35805CUPR-NF was designed to be an integral part of a public safety DAS network. Not only does it provide coverage for both cellular and Wi-Fi networks, it can provide low-band coverage allowing public safety services and first responders to stay connected within a specific location or structure during emergency situations,” said Ken Burgner, Product Manager.
With low-band operational coverage down to 380 MHz, this antenna supports UHF, 600 MHz, 1390-1432 MHz, AWS-3 bands and TETRA-compliant 2-way radios. It has a low-PIM rating of <-150 dBc which meets low-PIM requirements for LTE/4G bands and DAS applications. The multi-band design allows one antenna to be used for an array of in-building, wide-coverage wireless applications, which simplifies installation.
The HG35805CUPR-NF is designed to be aesthetically pleasing in almost any indoor environment. It can be easily mounted through a single 1.0 inch hole in a solid or suspended ceiling up to 1.2 inches thick. It features a 12 inch coax lead terminated with an N-Female connector. Special order connectors are also available.
For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, pmcneil@l-com.com
About L-com Global Connectivity:
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit:
https://www.L-com.com/