NORTH ANDOVER, MA – (May 24, 2011) – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, has developed a very compact 2.4 GHz multiple-input and multiple-output (MIMO) ceiling antenna designed to operate with many manufacturers' enterprise-class 802.11n MIMO access points (APs). This antenna features three integrated 2.4 GHz antennas in one enclosure, making it an ideal to support applications in next generation of IEEE 802.11n wireless communication systems. “The compact radome allows this antenna to be mounted in many areas where space is at a premium,” said Ken Burgner, product manager. This omni-directional antenna features spatial diversity between three independent antenna ports providing better wireless reception in areas susceptible to the effects of multi-path interference. Only 5.8” in diameter, this antenna is no bigger than a typical smoke detector, making it appealing for use in offices, health facilities, educational settings and retail complexes. For more information on this antenna, please call 1-800-341-5266. About L-com L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/. |