NORTH ANDOVER, Mass. (March 31, 2016) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has introduced a cross-polarized low-PIM DAS panel antenna.
L-com’s HyperLink® brand HG72708XWPPR-NF is a cross-polarized, directional wall mount MIMO panel antenna that is specifically designed for in-building wireless networks including DAS applications. The HG72708XWPPR-NF can provide coverage ranging from 700 MHz to 2700 MHz in a single antenna package. This enables it to support various networks including cellular 4G/LTE, Personal Communication Services (PCS), and 802.11b/g/n wireless networks. Combining many frequencies into a single antenna eliminates the need to purchase separate antennas for each wireless network type, simplifying installation and reducing deployment costs.
“Cross-polarization and simple installation make this DAS antenna ideal for providing wireless coverage in large, open areas such as indoor courtyards, indoor sporting venues, convention centers and shopping malls,” said Ken Burgner, Product Manager.
The HG72708XWPPR-NF features two independent antennas with cross-polarization, which doubles the wireless capacity over the same channels. The antenna is fed via two plenum-rated antenna leads terminated with N-female connectors. One antenna is +45° polarized and the other is -45° polarized, making this antenna ideal for polarization diversity systems.
With a PIM rating of <-150dBc, the HG72708XWPPR-NF is also low-PIM rated and meets the most demanding PIM requirements for the LTE/4G bands.
L-com also offers a full line of products for DAS networks such as low-loss cabling, fiber optic cabling, and surge protection.
For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, mailto:pmcneil@l-com.com
About L-com Global Connectivity:
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit: https://www.L-com.com/