NORTH ANDOVER, Mass. (October 13, 2016) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has released a series of GigE RJ45 Ethernet cable assemblies.
L-com now offers GigE RJ45 Ethernet cable assemblies specifically made for machine vision applications. The GigE connectors on our assemblies are built to meet the vision standard and are perfect for machine vision camera and PoE applications. Screw mount hardware provides a secure connection and is beneficial in many applications where standard RJ45 connectors can become dislodged due to jostling, vibration, gravity, etc.
These rugged assembles are built with L-com's outdoor-rated, industrial, high-flex cable for maximum durability and are excellent for outdoor, industrial or harsh network installations. These cables are also double-shielded to minimize EMI/RFI interference and feature a Flame-Retardant Thermoplastic Elastomer (FR-TPE) cable jacket to protect against oil, sunlight (UV) and weld splatter.
“L-com’s GigE RJ45 Ethernet cable assemblies are specifically designed to the specifications of the Automated Imaging Association (AIA) machine vision standards. As a member of AIA, customers can rest assured that our machine vision cable assemblies will mate when using any machine vision standard device,” said Dustin Guttadauro, Product Manager.
L-com's GigE Ethernet cables are available in GigE to GigE RJ45 and GigE to standard RJ45 configurations with either a Category 5e or Category 6a rating. Custom lengths, labeling, connector configurations and packaging are available.
For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, mailto:pmcneil@l-com.com
About L-com Global Connectivity:
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit: https://www.L-com.com/