NORTH ANDOVER, Mass. (November 12, 2015) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has developed a line of industrial NEMA-rated enclosures.
L-com’s NB20-series enclosures are molded from halogen-free, self-extinguishing, fiberglass reinforced polyester (FRP) to withstand extreme temperatures and wet and corrosive environments. They protect electrical and electronic components and equipment from water, wind, dust and chemicals, as well as preventing theft and damage. These enclosures feature fully gasketed lids and stainless steel quick-release latches with padlock hasps to lock the enclosure and secure the internal equipment.
“Protecting expensive electrical and electronic equipment is critical for any industry. L-com’s industrial NEMA-rated NB20-series enclosures provide the superior protection needed for sensitive equipment. Their large size of 20x16x11 inches provides sufficient space for multiple or large devices to be mounted inside,” said Ken Burgner, Product Manager.
The NB20-series features options, such as 120V AC power and non-powered configurations, as well as heating and cooling options. Approvals for the NB20-series include UL and NEMA ratings, IEC and CSA (ratings may vary from model to model).
For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, mailto:pmcneil@l-com.com
About L-com Global Connectivity:
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions and Aiconics®, a leading manufacturer of electrical connector products. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit: https://www.L-com.com/