To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Launches New 900 MHz UP-series Omni-Directional Antennas

Wednesday, April 19, 2017

NORTH ANDOVER, Mass. (April 20, 2017) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has released a new line of Omni-directional antennas for use with 900 MHz wireless LAN, SCADA, wireless video links and 900 MHz cellular band applications.

L-com’s new 900 MHz UP-series antennas are lightweight, low-profile, high-performance, Omni-directional antennas designed for the 900 MHz ISM band. They feature an integral N-female-type connector and a slim, 20 mm diameter, white, UV-stable, fiberglass radome for added durability. These antennas are designed with a sealed, aluminum end cap and drain holes at the base to help prevent condensation build-up inside the antenna, which helps ensure reliable performance.

“Our new high-performance 900 MHz UP-series antennas are ideal for multipoint, Non-Line of Sight (NLOS) and mobile applications where compact form factor, high-gain and wide-coverage is a requirement,” said Mark Blackwood, Product Manager.

These omni directional antennas feature a rugged, industrial-grade design for all-weather performance. They include a mast mounting kit that consists of an extruded aluminum bracket and a pair of U-bolts for installation on masts up to 2.0" in diameter. To ease installation, the bracket can be installed first without the antenna, which can then be mounted after the bracket is installed.
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
<!--[if gte mso 9]> <w:LsdException Locked=""false"" Priority=""52"" Name=""List Table 7 Color