L-com, an Infinite Electronics brand and a preferred manufacturer of wired and wireless connectivity products, announced today that it has introduced a new line of Category 7-rated Ethernet cable assemblies that provide high-speed voice, video and data connectivity to data centers, server farms, LANs and industrial networks where heavy EMI /RFI is present.
Four new cable series are offered that all feature double-shielded cable with overall braid shield around individually shielded twisted pairs (S/FTP) which keeps the overall cable diameter small. Additionally, these cables are 10 Gig and Category 7-rated, wired for Ethernet (TIA 568B) and are available in off-the-shelf lengths of 0.5 to 15 meters.
The TRD795ZBLU and TRD795ZBLK-series cables feature IEC-rated LSZH cable, and the TRD795BLU and TRD795BLK-series cables are constructed using UL CM-rated PVC cable. Both black and blue color options are available.
"Our new Category 7 cables offer the best of both worlds: high-speed Cat 7, 10 Gig connectivity and double shielding to thwart the data corrupting effects of EMI/RFI. Also, low-smoke, zero-halogen and PVC jacket options address a wide range of applications," said Dustin Guttadauro, Product Line Manager.
In addition to these new Ethernet cable assemblies, the bulk cable used to make these assemblies is also available for purchase.
L-com’s new double-shielded Cat7 cable assemblies are in-stock and available for same-day shipping.
About L-com:
L-com, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2015 certified and many of its products are UL® recognized. L-com is an Infinite Electronics brand.
About Infinite Electronics:
Based in Irvine, Calif., Infinite Electronics offers a broad range of components, assemblies and wired/wireless connectivity solutions, serving the aerospace/defense, industrial, government, consumer electronics, instrumentation, medical and telecommunications markets. Infinite’s brands include Pasternack, Fairview Microwave, L-com, MilesTek, ShowMeCables, NavePoint, INC Installs, Integra Optics, PolyPhaser, Transtector, KP Performance Antennas, RadioWaves & Aiconics. Infinite Electronics serves a global engineering customer base with deep technical expertise and support, with one of the broadest inventories of products available for immediate shipment.
###
Press Contact:
Peter McNeil
L-com
17792 Fitch
Irvine, Calif. 92614
978-682-6936