To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors

Wednesday, May 22, 2019

IRVINE, Calif. May 23, 2019 L-com, an Infinite Electronics brand and a preferred manufacturer of wired and wireless connectivity products, has just introduced two new Category 6a lightning and surge protectors to address 10/100/1000/10000 Ethernet applications.

The AL-CAT6AHPJW lightning and surge protector provides superior lightning and surge protection with improved frequency response for 10/100/1000/10000 Base-T Ethernet networks. It is designed for outdoor use and utilizes ultra-low capacitance semiconductors which provide superior high frequency response and improved return loss for the four data pairs.

L-com’s HGLN-CAT6AJ was designed to address quad-speed indoor surge protection applications and utilizes thyristor diode technology which offers superior power handling capability compared to TVS or Zener diode based designs. Additional features include our shielded RJ45 connector, backward compatibility with Cat6, Cat5e and Cat5 cabling and a rugged aluminum enclosure.

“Our new Cat6a lighting and surge protectors were developed to address both indoor and outdoor network installations where the need for high-speed 10 Gbps Ethernet connectivity is required. These robust surge protectors were designed to protect our customer’s valuable communications equipment from power surges and lightning strikes," said Dan Rebeck, Product Manager.

The new AL-CAT6AHPJW and HGLN-CAT6AJ surge and lightning protectors are in-stock and are available to ship immediately.

For inquiries, L-com can be contacted at +1-978-682-6936.

About L-com:
L-com, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. L-com is an Infinite Electronics brand.

About Infinite Electronics:
Infinite Electronics is a leading global supplier of electronic components serving the urgent needs of engineers through a family of highly recognized and trusted brands. Our portfolio brands are specialists within their respective product set, offering broad inventories of engineering-grade product, paired with expert technical support and same-day shipping. Over 100,000 customers across a diverse set of markets rely upon Infinite Electronics to stock and reliably ship urgently needed products every day.