To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Launches New Line of Coaxial RF Lightning and Surge Protectors

Tuesday, April 24, 2018

NORTH ANDOVER, Mass. (April 25, 2018) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has launched a new series of high performance, coaxial lightning and surge protectors developed to protect valuable communications equipment from indirect lightning strikes and power surges.

The LCSP-series surge protectors feature VSWR as low as 1.1:1, max power as high as 2kW, multi-strike capability, low insertion loss and are available with 4.3-10, 7/16 DIN, Type-N and UHF connectors. Furthermore, these RF surge protectors support a frequency range from DC to 6 GHz and are CE & RoHS compliant. The majority of these new surge protectors are IP67-rated for outdoor use and some models offer low-PIM performance. Additionally, models are available with flexible bulkhead or bracket mounting options.

These new coaxial RF surge and lightning protectors can be used in Wi-Fi networks, cellular base stations, active antenna systems, DAS networks and public safety systems.

“L-com’s new coax surge protectors were developed using a proprietary surge technology that provides fast responses to power and lightning surges. These new surge protectors deliver high RF performance while protecting critical infrastructure devices found in a variety of wired and wireless network deployments,” said Steven Pong, Product Manager.

L-com’s new coaxial lightning and surge protectors are in stock and available for immediate shipment.
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
L-com Global Connectivity, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. L-com is an Infinite Electronics company.

Search Entries: