To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Launches New USB 3.0 High-Flex Cable Assemblies

Wednesday, October 4, 2017

NORTH ANDOVER, Mass. (October 5, 2017) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has introduced a new series of high-flex USB 3.0 cable assemblies for use with PC peripheral interconnects, data acquisition, test and measurement and portable data storage applications.

These new USB 3.0 high-flex cables are rated for 10,000 flex cycles, making them ideal for applications where standard USB 3.0 cables fail. They are available with three connector options: Type-A male to Type-A male, Type-A male to Type-B male and Type-A male to Micro-B male. These high-flex cables feature a TPE cable jackets and 30 AWG high strand count conductors. Additionally, a foil plus braid shield provides maximum protection against EMI/RFI.

The Type-A to Type-A and Type-A to Type-B cables are available in 0.3, 0.5, 0.75, 1 and 1.5-meter lengths and the Type-A to Micro-B cables are available in 0.3, 0.5, 0.75-meter lengths.

“These exclusive, ultra-flexible USB 3.0 cables were specifically designed to address applications where ordinary cables fail due to excessive flexure. They can withstand 10 times as many bend cycles as a standard cable while retaining their durability and performance,” said Brian Gates, Product Manager.

L-com’s USB 3.0 high-flex cable assemblies are in stock and available for immediate shipment.
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
L-com Global Connectivity, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. L-com is an Infinite Electronics company.

Search Entries: