L-com, an Infinite Electronics brand and a preferred manufacturer of wired and wireless connectivity products, announced today that it has launched a new series of ruggedized USB 3.0 cables that feature die-cast metal back shells and optional thumbscrews that are commonly used in machine vision applications.
L-com’s new CAU3DCVIS-series cables were developed to address demanding connectivity applications including industrial and factory automation, process engineering, machine vision, data acquisition and PLC communications.
These unique and hard to find cables feature specialized die-cast back shells with optional thumbscrews for securing the connectors to ensure connectivity is not disrupted in the event of pull or impact. The cables are available off-the-shelf with the following connector combinations: Type-A male to Micro-B male, Type-A male to Type-C male and Type-A male to Type-B male. Other features include black PVC cable jackets, double shielding and 22AWG power conductors which provide maximum USB power transfer.
“Our new ruggedized USB 3.0 cables are perfect for use in industrial settings where high vibration, impacts and other harsh conditions prevail. These unique cables can be mated to any standard USB 3.0 Type-A jack and allow for the use of thumbscrews for applications requiring extra secure connections,” said Dustin Guttadauro, Product Line Manager.
L-com’s new ruggedized USB 3.0 cable assemblies with die-cast back shells are in-stock and available for immediate shipment.
About L-com:
L-com, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2015 certified and many of its products are UL® recognized. L-com is an Infinite Electronics brand.
About Infinite Electronics:
Based in Irvine, Calif., Infinite Electronics offers a broad range of components, assemblies and wired/wireless connectivity solutions, serving the aerospace/defense, industrial, government, consumer electronics, instrumentation, medical and telecommunications markets. Infinite’s brands include Pasternack, Fairview Microwave, L-com, MilesTek, Aiconics, KP Performance Antennas, PolyPhaser, Transtector, RadioWaves, ShowMe Cables, INC-Installs and Integra Optics. Infinite Electronics serves a global engineering customer base with deep technical expertise and support, with one of the broadest inventories of products available for immediate shipment.
###
Press Contact:
Peter McNeil
L-com
17792 Fitch
Irvine, CA
978-682-6936