L-com Launches TS-9 Coax Connector and Antennas
NORTH ANDOVER, MA - 04/10/14 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, announced today that they will now be offering TS-9 Plug Crimp Connectors as well as two new HyperLink® Range Extender Antennas (which feature TS-9 Connectors). The TS-9 crimp connector is a small coax connector that is commonly used with cellular phone products and not generally found among large wireless distributors.
"Since the TS-9 is typically a hard-to-find connector, we're excited that we can provide a solution for those customers who need it," said Kenneth Burgner, Product Manager.
The L-com 50 Ohm TS-9 coax connector, ATS9P-1100, is a TS-9 plug crimp connector that is designed for use with a low-loss 100-series cable such as L-com's CA-100. It can also be used with RG316, RG188 and RG174 cables. It features nickel-plated brass construction for maximum durability. In addition to being offered individually, the ATS9P-1100 is available through L-com's on-line custom cable configurator for 100-Series low-loss cables.
L-com's new HyperLink® range extender antennas, RE905U-TS9 and RE1903U-TS9, are ideal for use with 900 MHz cellular products that have external antenna ports and feature the TS-9 connector. These antennas help to increase the range that is typically offered by the internal antennas found in cellular products. Made for both indoor and outdoor applications, the antennas also feature a magnetic mounting system with attached four- foot cable.
Among a variety of cellular product applications, the TS-9 connector and the range extender antennas can be used with PC cards, mobile phones, wireless LAN products, laptops and more.
For more information about this release, please contact:
Peter McNeil, Product Marketing Manager
978-682-6936 x1450, pmcneil@l-com.com
L-com Global Connectivity, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com's other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions and Aiconics®, a leading manufacturer of electrical connector products. Trusted for over 30 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit: https://www.L-com.com/###