NORTH ANDOVER, Mass. (2/25/16) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it now offers USB 2.0 Micro-B and Mini-B 5 position LSZH cable assemblies.
L-com's LSZH USB cable assemblies are designed for use in areas where toxic smoke from standard cables could damage sensitive equipment and for use in enclosed areas where air quality is a concern. These cables are also a cost effective solution for installations that prohibit the use of PVC and utilize Micro-B and Mini-B 5 position USB connectors.
“When an application calls for the restriction of PVC, L-com provides our customers the ability to source and install cables in full compliance without sacrificing quality or availability,” said Dave Gallagher, Product Manager.
These new cables feature double-shielded 28/28 AWG LSZH cabling, 30u gold plated connectors that stand up to repeated mating cycles and LSZH jackets and over molds. They are available in five off-the-shelf lengths from 0.3 meters to 3 meters.
For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, mailto:pmcneil@l-com.com
About L-com Global Connectivity:
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit: https://www.L-com.com/