NORTH ANDOVER, MA – 6/30/2010 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, announced today it now has achieved UL Listing for the following Industrial Enclosures:
NB121005 | 12"x10"x5", No Mounting Plate - UL LISTED |
NB141207 | 14"x12"x7", No Mounting Plate - UL LISTED |
NB141207-01-UL | 14"x12"x7", Drilled Mounting Plate - UL LISTED |
NB141207-100-UL | 14"x12"x7", Mounting Plate, 120VAC Sockets - UL LISTED |
NB141207-100T-UL | 14"x12"x7", Mounting Plate, 120VAC Terminal Block - UL LISTED |
NB141207-10FS-UL | 14"x12"x7", Mounting Plate, 120VAC Fan, Solid State Controller - UL LISTED |
NB141207-1HFS-UL | 14"x12"x7", Mounting Plate, 120VAC Fan, Heater, Solid State Controller - UL LISTED |
NB181608 | 18"x16"x8", No Mounting Plate - UL LISTED |
Underwriters Laboratories (UL) is the trusted resource across the globe for product safety certification and compliance solutions. Many companies will require a UL Listing on products they purchase to assure the quality and safety of that product. | |
“The standard of consumer safety is the UL Listing you may have seen on other products,” said Karl Blomgren, L-com’s Product Manager for Industrial Enclosures. “We want to assure our customers that when they require UL Listed enclosures they can buy with confidence, products that have met the UL criteria for safety and quality.”
The new UL Listed products are available now from L-Com and may be ordered under the part numbers listed nearby. Blomgren mentioned that this move illustrates the power of customer collaboration, as the UL Listing is often required for use in installations to ensure user safety.
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.
https://www.L-com.com/