NORTH ANDOVER, MA, -- January 15, 2010 -- L-com Global Connectivity, a leader in both wired and wireless connectivity products, announced today that it has started to carry one foot long SVGA to Quick Disconnect cables. These cables are used as spares or replacements for the ones that come with L-com's popular quick disconnect SVGA cables.
The "quick disconnect" feature on L-com's ultra-flexible Super Thin line of SVGA cables was originally created to allow easy connection in a tight gang-box behind a wall. The disconnect side is only 0.75" wide, allowing it to pass through conduit and pipes that are too thin for an SVGA connector.
These new spare one-foot cables complete the already extensive line of disconnect feature cables.
L-com now supplies:
L-com has made a name for itself in the global connectivity market as both an innovator and one-stop-shop for connectivity products. The addition of this part helps to enforce this reputation.
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized. https://www.L-com.com/