NORTH ANDOVER, Mass. (July 14, 2016) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it now offers two series of Brad® cable assemblies: the Ultra-Lock® M12 and Nano-Change® M8.
“We are excited to offer the Brad® Ultra-Lock® M12 and Nano-Change® M8 cable assemblies directly to our customers, and at a better price than most competitors. The M12 and M8 cables perfectly complement L-com’s industrial product line and feature a rugged design that will withstand the harshest conditions while maintaining optimal performance and protection against liquids and particulates,” said Dustin Guttaduaro, Product Manager.
Brad® Ultra-Lock® M12 cable assemblies provide a fast, simple and secure operator-independent connection. They feature Ultra-Lock® connectors with a unique radial seal and mechanical-locking design that locks with a quick push-pull motion to guarantee a secure seal every time. These M12 cable assemblies are designed to eliminate connector-related intermittent signals in the harshest environments, which can mean less downtime and increased productivity. When the cables are mated, an IP69K rating provides protection against liquids and particulates even in wash-down or submerged applications. These rugged cable assemblies feature cost-effective PVC jackets, 22AWG conductors as well as 4-position and 5-position A-coded connector options.
Brad® Nano-Change® M8 cable assemblies are designed to be rugged and compact, making them ideal for use with miniature sensors and actuators used in industrial control applications. They are built with IEC-compliant M8 Nano-Change® connectors that are designed to withstand harsh industrial environments and utilize an anti-vibration feature to prevent loosening in high-vibration applications. When the cables are mated, an IP68 rating provides protection from liquids and fine particulates. These M8 cable assemblies feature cost-effective PVC jackets and a dynamic -20°C to +105°C operating temperature range. They are available with both 3-pole and 4-pole connector options.
For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, pmcneil@l-com.com
About L-com Global Connectivity:
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit: https://www.L-com.com/