North Andover, MA – July 3, 2007 – L-com Connectivity Products announced today that it now offers HDMI cable assemblies in longer length and in direct panel mount versions. These cables are ideal for applications that require longer runs than the typical five meter cables that are often found in the marketplace. By using heavy gauge 24AWG and 22AWG conductors, L-com’s cables can achieve lengths as long as 90 meters with the assistance of L-com’s HDMI signal boosters. Their new HDMI female panel mount cable assembly can be directly mounted to a panel or wall plate without the need of a feed thru adaptor. Here are the three versions that are available:
CTL-L-HDMI-XX Series with lengths up to 45 meters (147.6 feet) CTL-XL-HDMI-XX Series with lengths up to 90 meters (295.2 feet) CTL-PM-HDMI-XX Series unique panel mount HDMI female connectors For more information about this release, please contact:
David Dolce, Product Marketing Manager 978-682-6936 x161, ddolce@L-com.com For over 25 years, L-com Connectivity Products has designed, manufactured, and distributed an extensive offering of copper and fiber telecom and datacom interconnect components such as cable assemblies, adapters, couplers, and connectors, in addition to custom product design and manufacturing capabilities. L-com is headquartered in North Andover, Massachusetts. For more information please visit www.L-com.com. |