NORTH ANDOVER, MA – 6/4/15 – L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has released a series of panel-mount USB couplers with high-retention connectors.
L-com's high retention ECF-style panel-mount USB couplers were developed to address USB connectivity application requirements in environments where vibration and cable pull may occur. The specialized high-retention connectors used in these couplers offer a mating force of 40N max and an un-mating force of 15N min, which is 50% higher than standard USB connectors.
The couplers are available in USB Type B-A, A-A, and A-B connector configurations and feature shielded housings, which limit the effects of EMI/RFI often found in industrial environments.
“Our high-retention USB couplers were designed for use in industrial USB applications where vibration and accidental cable pull may occur. The panel-mount style allows the couplers to be used in enclosures, panels and other designs where a feed-through USB coupler is required,” said Steve Smith, Product Manager.
For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, mailto:pmcneil@l-com.com
About L-com Global Connectivity
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions and Aiconics®, a leading manufacturer of electrical connector products. Trusted for over 30 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit: https://www.L-com.com/