To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Now Offers Lightning and Surge Protection for Harsh Environments

Wednesday, November 10, 2010

NORTH ANDOVER, MA – 11/11/2010 – L-com, Inc, a global leader in the manufacture of wired and wireless connectivity products, now offers a lightning and surge protector featuring an industrial-grade die cast aluminum enclosure with a gasketed cover and concealed mounting holes. This “ALW” series is designed for the harshest of environments.

“L-com’s lightning and surge protection product offering was already quite extensive,” said Ken Burgner, Product Manager for lightning protectors, “but until now we had very limited industrial solutions. The new ALW solves lightning and surge-related issues in environments where surge protectors cannot normally help.”

L-com currently offers eight models in the ALW series but plans to add more models by year’s end including its new 4 to 20 mA current loop protectors. The current offering includes:

Lightning and surge protectors are designed to protect sensitive wired and wireless systems from the damage that can result from lightning strikes and power surges. 

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com


L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.