NORTH ANDOVER, MA – 3/2/2010 – L-com Global Connectivity, a leading manufacturer of wired and wireless connectivity products, announced today that it now offers M12 cables, connectors and adapters for use in industrial Ethernet and fieldbus applications.
The M12 cable series includes both D and A coded connectors with male, female, and 4 or 5 position options. L-com’s M12 cables feature UV and chemical resistant PUR jackets as well as rugged 22 AWG conductors.
In addition to the M12 cables, L-com now stocks panel mount, PCB, and solder style D-coded M12 connectors with both 4 and 5 position options.
To round out L-com’s new M12 product offering, they have also introduced a line of M12 cable adapters in T, I, and Y style configurations.
To complement their new M12 products, L-com also offers a wide variety of Industrial rated RJ45 Ethernet cables for process industry and factory automation applications.
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.
https://www.L-com.com/