To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications

Wednesday, March 20, 2019

IRVINE, Calif. (March 21, 2019) - L-com, an Infinite Electronics brand, and a preferred manufacturer of wired and wireless connectivity products, announced today that it has introduced a new series of 12G-SDI BNC connectors to address professional broadcast video applications.

L-com’s new V7C0000-series 12G-SDI connector line consists of models with both BNC and ultra-tiny BNC interfaces to address a host of HD video applications. 12G is a Serial Digital Interface (SDI) standard developed to support greater resolution, frame rates and color fidelity. It provides four times the bandwidth of HD, supporting up to12Gbps, making it ideal for the 4Kp60 format.

These 75 Ohm, 12G-SDI connectors enable transmission of high resolution uncompressed video signals and offer 4K and Ultra HD quality signals. Connector package options include PCB-style, end-launch and straight-style 12G-SDI connectors.

Search Entries: