NORTH ANDOVER, Mass. (July 19, 2018) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has introduced a new series of right angle connector M12 cable assemblies to address harsh environment Ethernet connectivity applications.
These new right angle M12 cable assemblies were designed to address demanding industrial connectivity requirements in confined spaces where standard straight connectors will not fit. Built with high flex, outdoor CMX rated, double shielded, FR-TPE cable and using IP67 rated M12 connectors, these M12 assemblies can be used in harsh environments where exposure to oil, UV rays and weld splatter is present.
The TRG507-T4T series features a straight M12, 4 position, D-coded connector on one end of the assembly and a right angle, M12, 4 position, D-coded connector on the other end. The TRG508-T4T series features a right angle, M12, 4 position, D-coded connector on one end of the assembly and a shielded RJ45 connector on the other end.
“Our new right angle M12 cable assemblies were developed to address confined space connectivity applications in industrial settings where standard straight connectors will not fit. These new right angle M12 cables complement our extensive line of M12 series cables that offer many different connector and cable jacket options,” said Dustin Guttadauro, Product Manager.
L-com’s new right angle M12 cable assemblies are in stock and can be shipped immediately.
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
L-com Global Connectivity, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. L-com is an Infinite Electronics company.